Press releases

Vacuum Components

10.10.2011
700 Pages on Vacuum Components and Much More

Schmalz presents the greatest variety of vacuum components the market has to offer in its new Vacuum Components Catalog 2012/2013.

15.06.2011
Turning Two into One: Safely Separating Double Blanks

When automatically feeding raw sheets, sheet metal parts, blanks and other flat workpieces into forming machines, it is important to separate components and ensure that they are fed in individually to prevent damage to the machines. In conjunction with commercially available sensors, the double-blank detection unit DBD from vacuum technology specialist J. Schmalz does just that – precisely and reliably.

10.05.2011
Configured in no time

Vacuum technology specialist J. Schmalz presents the first modular system for fast and easy setup of vacuum end effectors for the packaging industry

all articles


Vacuum Gripping Systems

27.07.2011
1200 suction pads close gap in automation process

With a gripping system consisting of 1200 packaging suction pads, Vacuum specialist Schmalz has closed one of the few gaps in the automation process of Deutsche Post’s logistics centers. The system provides maximum flexibility and holding force in a robot cell for automatic depalletizing and separating of cardboard boxes.

04.04.2011
New for PV Production: the SSG String Gripper from Schmalz

The logical next step – vacuum specialist Schmalz has added the SSG string gripper to its product range for the photovoltaic process chain and presents for the first time a modular gripping system especially for handling PV strings.

06.08.2010
Automatic is better: Robot-assisted palletizing with a vacuum gripper system

A renowned manufacturer of built-in kitchen appliances utilizes a robot with a vacuum gripper system for flexible and economical handling and palletizing of packaged range hoods.

all articles


Vacuum Handling Systems

25.04.2012
Lightweight Crane Systems

The aluminum crane systems SRA from Schmalz are distinguished by their consistently lightweight design. The standardized components allow for cost-effective implementation of individual material flow solutions.

17.10.2011
Suction Power instead of Muscle Power

Vacuum tube lifters facilitate efficient inverter production - With its new production facility, the inverter specialists at KACO new energy are setting a course for the future. The switch to fully automatic processes and order-specific production requires a smooth material flow. In places that still require manual handling of the heavy inverters, employees will now have help from multiple vacuum tube lifter JumboErgo units from Schmalz. These units are well-suited to the ergonomic concept of the production facility.

14.10.2011
New: Crane Systems with Wireless Power Supply and Increased Load Capacity

Specialists in vacuum handling technology J. Schmalz are presenting two crane system innovations: a conductor line for wireless power supply and a crane section that can carry loads weighing up to 950 kg.

all articles


Vacuum Clamping Systems

03.06.2011
It Doesn't Always Have to Be the Original

Vacuum technology specialist Schmalz offers affordable replacement suction pads for SCM/Morbidelli console systems.

20.05.2011
XXL Flexibility for Clamping Workpieces

New from Schmalz: The Innospann adapter plate XXL increases the flexibility with which users can attach suction cups to CNC machining centers with a console table.

24.02.2011
The New Brochure – “Vacuum Clamping Systems” from Schmalz

In a new 36-page brochure, J. Schmalz GmbH presents innovative clamping solutions for CNC machining centres.

all articles


Company

12.03.2012
Schmalz is recognized as one of “Germany’s Best Employers” for the third time

The employees of J. Schmalz GmbH in Glatten had every reason to celebrate. The reason: they work for one of “Germany’s Best Employers 2012.” This has been published in a ranking by the “Great Place to Work Institute Deutschland”.

08.06.2011
Schmalz Wins Prize for the “Best Assembly Idea 2011”

In June 2011, the vacuum specialist J.Schmalz was awarded for its "Pick-by-Shutter" assembly workstation. This workstation is used to assemble ejectors from individual components. This particularly innovative solution leads to sustainable improvements in efficiency and working conditions.

01.03.2011
South Korea Is Most Successful Schmalz Company for 2010

To start off the year, Schmalz held its World Market Meeting at its headquarters in Glatten. The company used this opportunity to greet the managing directors of its 16 international subsidiaries. As in years past, the subsidiary that showed the strongest growth was acknowledged.

all articles



Altre informazioni:

Not a "Italian" Visitor?

Kein "italienischer" Besucher?

Schmalz weltweit:

Verifica la disponibilità ed prezzo
Componenti per il vuoto, sistemi di bloccaggio e Attrezzatura per l’officina


Ordinazione diretta


Carrello

0Posizioni 0,00 €

Fiere

Ogni anno Schmalz presenta le sue novità in numerose fiere.

Di più...